SLAU292G November 2009 – July 2015
Press * until the heart icon appears on the display that is heart rate mode is active (see Figure 3-1 for details). When this mode is active, heart rate is shown and burned calories are determined (additional settings must be made for first time use, see Section 3.2.2.7). For information on how to use the chest belt, see to the documentation included with the heart-rate monitor device.
NOTE
This mode requires a heart-rate monitor (chest belt) that is not included in this kit, but available from BM innovations, Germany (see www.bm-innovations.com/chronos). However, a heart rate can be simulated without a chest belt by the eZ430-Chronos Control Center, see Section 3.3 for details.
While almost all other eZ430-Chronos functions are based on TI's SimpliciTI protocol, the heart-rate monitoring uses BlueRobin, an ultralow-power low-data-rate wireless communication protocol from BM innovations.
Secondary function: Heart rate display on/off. Press UP to enable or disable the heart-rate monitoring. Once a connection is established, the heart rate is shown on the top LCD line
Set function: None