2.3.1 Transmission of Acceleration Data and Button Pushes
Select the SimpliciTI Acc/PPT tab.
Click Start Access Point to start PC. When the PC is ready, the control center status line displays "Access point started. Now start watch in ACC, PPT or synch mode".
Select the ACC mode in the bottom LCD line of the eZ430-Chronos module and active the data transmission by pressing the DOWN button. The Chronos module connects to the PC (this may take a few seconds) and starts transmitting 3-Axis acceleration values
After connection, the Control Center status bar reports "Receiving data from acceleration sensor" and the values according to the axis. The graphs display the acceleration data of the Chronos module for each axis.
Figure 2-5 eZ430-Chronos Control Center With Acceleration Data