SLAU292G November 2009 – July 2015
This access point consists of an MSP430F5509 microcontroller connected to a <1-GHz transceiver (CC1101) (see Figure 4-12).
As shown in Figure 3-15, the RF access point can be reprogrammed by connecting the eZ430 USB emulator to the access point. First of all, solder the 4-pin debugger connector (provided with the kit) onto the access point.