SLAU292G November 2009 – July 2015
In this mode, the Chronos module constantly transmits acceleration data to the PC. In addition, #, *, and UP button pushes are transferred. The Control Center software shows the 3D acceleration in graphs. Optionally, mouse control can be activated by clicking on Mouse On (M) or by typing M on the keyboard.
Once active, the PC mouse pointer can be controlled by tilting the Chronos module. Hold the Chronos module with its display facing up. The mouse pointer moves vertically (X-axis in Control Center) when tilting the wrist module forward or backward and move vertically (Y-axis in Control Center) when tilting it left or right. Mouse clicks are also possible–see the following description. Mouse control can be calibrated (to set a point of zero acceleration or no pointer movement) by selecting Calibration (C). It may be disabled by clicking Mouse Off (M) or by typing M on the PC keyboard.
NOTE
Holding buttons (for example, to drag and drop) is not supported.
Turn the demo off by pushing the DOWN button on the eZ430-Chronos module and clicking "Stop Access Point" in the PC application.
Figure 3-3 eZ430-Chronos Control Center With Acceleration Data