SLAU292G November 2009 – July 2015
This mode requires the eZ430-Chronos Control Center PC software.
Press # until PPt is shown (see Figure 3-1). This mode allows control of a PowerPoint presentation by translating button pushes on the Chronos module into keystrokes of the PC keyboard. No acceleration or other data is transmitted. The default settings are:
The Control Center allows user defined key settings (including combinations) (see Section 3.3.2).
Secondary function: Start or stop transmission of button pushes. Pushing DOWN starts/stops the pairing process or stops the transmission (the access point on the PC must be started from the eZ430-Chronos Control Center (see Section 3.3.1). The RF icon on the LCD flashes when the radio is active; if pairing fails, the icon disappears. The top LCD line shows the time during the pairing until the data transmission is disabled.
Set function: None