The eZ430-Chronos access point USB drivers are included in the eZ430-Chronos installer package. A separate driver wizard window opens during installation as shown in Figure B-1. Continue by clicking next. A Windows warning may appear as the driver is not certified. Accept the driver installation.
Figure B-1 Device Driver installation Wizard for the Access Point
The driver installation wizard shows if the driver is successfully installed (see Figure B-2)
Figure B-2 Successful Driver Installation for Access Point
Insert the access point.
Windows detects the new hardware as TI CC1111 Low-Power RF to USB CDC Serial Port or eZ430-ChronosAP (see Figure B-3).
Figure B-3 Access Point Detection for eZ430-Chronos With Black PCB
Figure B-4 Access Point Detection for eZ430-Chronos With White PCB
Windows may open the Found New Hardware Wizard. If so, select No, not this time (see Figure B-5).
Figure B-5 Windows Found New Hardware Wizard
Select Install the software automatically in next dialog (see Figure B-6).
Figure B-6 Automatic Driver installation
A Windows warning appears as the driver is not certified. Click Continue Anyway (see Figure B-7). The drivers are installed.
Figure B-7 Windows Uncertified Driver Installation Warning
The Windows Device Manager lists the device TI CC1111 Low-Power RF to USB CDC Serial Port (COMx) or eZ430-ChronosAP (COMx) in Ports (COM & LPT) (see Figure B-8).
Figure B-8 Access Point in Windows Device Manager for eZ430-Chronos With Black PCB
Figure B-9 Access Point in Windows Device Manager for eZ430-Chronos With White PCB