SLAU292G November 2009 – July 2015
Press * until the "mi/h" or "km/h" icon is shown on the display; that is, the speed mode is active (see Figure 3-1). Your running speed is shown on the LCD top line.
NOTE
This mode requires a heart-rate monitor (chest belt) which includes an accelerometer to determine running speed. Visit BM innovations at www.bm-innovations.com/chronos for available additions. However, speed can be simulated without a chest belt by the eZ430-Chronos Control Center, see Section 3.3.4 for details.
While almost all other eZ430-Chronos functions are based on TI's SimpliciTI protocol, the speed mode uses BlueRobin, an ultralow-power low-data-rate wireless communication protocol from BM innovations.
Secondary function: None
Set function: None