SLAU292G November 2009 – July 2015
The eZ430-Chronos kit includes an USB emulator that provides full programming and debugging features using its Spy-Bi-Wire (2-wire) interface. It features a back channel MSP430 application UART that may be used independently of a debug session.
NOTE
The eZ430 USB emulator with white or black PCB are identical from a hardware perspective.
Despite the fact that the Chronos module is equipped with a 6-pin connector, there is no UART connection from the Chronos module to the emulator as all pins of the CC430 are already used for other purposes.
Supported devices:
Connector J1 on the emulator (starting on top with pin 1) (see Figure 4-14).