SLAU292G November 2009 – July 2015
NOTE
Only insert Q-LITE Lithium battery type CR2032 or equivalent.
CAUTION
Be careful when inserting the Chronos module. Do not push in the Chronos module or tighten the screws without checking if the module is in position. The metal strips of the buttons may get stuck at the buttons of the Chronos module housing. If this happens, gently push the strips towards the module with the screwdriver until they slide over the buttons (see Figure 4-6).