SLAU292G November 2009 – July 2015
Press * until the alarm mode is active (see Figure 3-1 for details). The alarm mode can be distinguished from time mode by an alarm symbol (bell) that flashes when the alarm time is displayed.
Secondary function: Alarm on or off. Press UP to enable or disable the alarm. The settings are confirmed by "on" and "off" in the top LCD line. The bell icon stays on in all other modes when the alarm is enabled and does not appear when the alarm is disabled.
Set function: Setting the alarm time.
NOTE
If no button is pressed for more than 30 seconds, the previous settings are restored.