SLAU292G November 2009 – July 2015
Press # until the "kcal" icon appears (see Figure 3-1). This mode shows the amount of calories that were burned while exercising, if the optional chest belt is used and heart rate mode is active. This mode also provides the distance (for example, when running) if a chest belt with build-in accelerometer is used. For accurate calorie determination, users need to set their sex and weight.
Secondary function: Distance. Press DOWN to activate the alternative display. To return to Calorie Mode, push the DOWN button again.
Set function: (Re-)setting calories and setting user weight and sex.
NOTE
If no key is pressed for more than 30 seconds, the previous settings are restored.