SLAU292G November 2009 – July 2015
The eZ430-Chronos PC software consists of a TCL/Tk executable and a DLL, which handles the communication with the RF access Point. Download TCL/Tk for Windows for free from http://www.activestate.com/activetcl. Once TCL/Tk was installed on the computer, a double-click on a TCL script (*.tcl) starts the interpreter and executes the script. Alternatively, start the TCL interpreter wish.exe and execute the script with the "source" command. If the script filename contains blanks, put it into quotes. The sources files are located in C:\Program Files\Texas Instruments\eZ430-Chronos\Control Center\GUI Sources