3.6.3.4.1.2 Access Point Based on CC1111
The CC Debugger is required to program the CC1111 based RF access point. To perform the update, the SmartRF Flash Programmer software is used to on the PC.
- Solder a debug interface connector cable onto the CC1111 access point as shown in Figure 3-16.
CC-Debugger |
RF Access Point |
Pin 1 |
GND |
Pin 2 |
Vcc |
Pin 3 |
P2.2 (DC) |
Pin 4 |
P2.1 (DD) |
Pin 7 |
RST |
Pin 9 |
Vcc |
- Connect RF access point to CC Debugger and press the "Reset". The LED on the CC Debugger should become green.
- Launch the SmartRF Programmer software
- Open .hex file according to frequency in C:\Program Files\Texas Instruments\eZ430-Chronos\Recovery\RF Access Point
- Select "Erase, program and verify"
- Clock "Perform actions"