SLAU292G November 2009 – July 2015
Press * until the tilt mode is active (see Figure 3-1). The acceleration is shown in G (9.81 m/s2) for all three axes. After entering the tilt mode, the y-axis acceleration is shown by default, and the z-axis or x-axis can be selected. Positive acceleration values are marked with a small arrow pointing up in the top LCD line, left of the acceleration. Negative acceleration values are marked with a small arrow pointing down. After 60 minutes, a timeout deactivates the measurements.
Secondary function: Select axis. The default is y-axis, followed by z-axis and x-axis.
Set function: None