SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
In IDLE mode, the watchdog interrupt (WDINT) signal can generate an interrupt to the CPU to take the CPU out of IDLE mode. As with any other peripheral, the watchdog interrupt triggers a WAKE interrupt in the PIE during IDLE mode. User software must determine which peripheral caused the interrupt.
Note: If the watchdog interrupt is used to wake-up from an IDLE low power mode condition, software must make sure that the WDINT signal goes back high before attempting to reenter the IDLE mode. The WDINT signal is held low for 512 INTOSC1 cycles when the watchdog interrupt is generated. The current state of WDINT can be determined by reading the watchdog interrupt status bit (WDINTS) bit in the SCSR register. WDINTS follows the state of WDINT by two SYSCLKOUT cycles.
In HALT mode, the internal oscillators and watchdog timer are kept active if the user sets CLKSRCCTL1.WDHALTI = 1. A watchdog reset can wake the system from HALT mode, but a watchdog interrupt cannot.