SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
FILE: hic_ex3_config_16bit_fsi.c
Example sets up Host Interface Controller Module in 16-bit mode the FSI Memory region of device is accessed by the External Host. This follows example configuration for performance critical applications described in the Application note titled "Application guide for peripheral expansion using HIC"(SPRACR2).
emif_ex7_16bit_asram_hic_fsi is to be run on the host before running this example on F28002x side.
This example is validated on an TI Internal Validation Platform will not run in F28002x Control Card
External Connections
This is tested on TI Internal validation platform hence no connection needed on Control card. This has been tested with F2838x EMIF interface.
Watch Variables
None - Use the Host to access FSI region