SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
FILE: lin_ex6_detect_incomplete_header.c
This example demonstrates how an error in the header field of a LIN frame can be detected. It configures the LIN module in responder mode and waits till new frame is received. It configures an external interrupt to trigger by a falling edge in the LIN Rx pin confirming start of frame. In the ISR of XINT, a timer is configured to trigger after max time consumed by reception of a complete LIN frame. If a LIN frame is successfully received the timer is disabled before getting triggered in the LIN ISR else the timer ISR is called which indicates an error in header frame.
External Connections
Watch Variables