SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
Table 3-56 lists the memory-mapped registers for the WD_REGS registers. All register offset addresses not listed in Table 3-56 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
22h | SCSR | System Control & Status Register | EALLOW | Go |
23h | WDCNTR | Watchdog Counter Register | EALLOW | Go |
25h | WDKEY | Watchdog Reset Key Register | EALLOW | Go |
29h | WDCR | Watchdog Control Register | EALLOW | Go |
2Ah | WDWCR | Watchdog Windowed Control Register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-57 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
W1C | W 1C | Write 1 to clear |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
SCSR is shown in Figure 3-49 and described in Table 3-58.
Return to the Summary Table.
System Control & Status Register
It is recommended to only use 16 bit accesses to write to this register. Use a read-modify-write instruction may inadvertently clear other bits.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | WDINTS | WDENINT | WDOVERRIDE | ||||
R-0-0h | R-1h | R/W-0h | R/W1C-1h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-3 | RESERVED | R-0 | 0h | Reserved |
2 | WDINTS | R | 1h | Watchdog Interrupt Status This bit indicates the state of the active-low watchdog interrupt signal (synchronized to SYSCLK). If the watchdog interrupt is used to wake the system from a low-power mode, then that mode should only be entered while this bit is high. Likewise, this bit must go high before the watchdog can be safely disabled and re-enabled. Reset type: SYSRSn 0h (R/W) = The watchdog interrupt signal is active. 1h (R/W) = The watchdog interrupt signal is inactive. |
1 | WDENINT | R/W | 0h | Watchdog Interrupt Enable/Reset Disable This bit determines whether the watchdog triggers an interrupt (WAKE/WDOG) or a reset (WDRS) when the counter expires. Reset type: SYSRSn 0h (R/W) = Counter expiration triggers a reset. This is the default state on power-up and after any system reset. 1h (R/W) = Counter expiration triggers an interrupt. |
0 | WDOVERRIDE | R/W1C | 1h | If this bit is set to 1, the user is allowed to change the state of the Watchdog disable (WDDIS) bit in the Watchdog Control (WDCR) register. If the WDOVERRIDE bit is cleared, by writing a 1 the WDDIS bit cannot be modified by the user. Writing a 0 will have no effect. If this bit is cleared, then it will remain in this state until a reset occurs. The current state of this bit is readable by the user. Reset type: SYSRSn |
WDCNTR is shown in Figure 3-50 and described in Table 3-59.
Return to the Summary Table.
Watchdog Counter Register
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
WDCNTR | |||||||
R-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R-0 | 0h | Reserved |
7-0 | WDCNTR | R | 0h | Watchdog Counter These bits contain the current value of the watchdog counter. This counter increments with each WDCLK (INTOSC1) cycle. If the counter overflows, either an interrupt or a reset is generated based on the value of the WDINTEN bit in the SCSR register. If the correct value is written to the WDKEY register, this counter is reset to zero. Reset type: IORSn |
WDKEY is shown in Figure 3-51 and described in Table 3-60.
Return to the Summary Table.
Watchdog Reset Key Register
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
WDKEY | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R-0 | 0h | Reserved |
7-0 | WDKEY | R/W | 0h | Watchdog Counter Reset Writing 0x55 followed by 0xAA will cause the watchdog counter to reset to zero, preventing an overflow. Writing other values has no effect. Reads of this register return the value of the WDCR register. Reset type: IORSn |
WDCR is shown in Figure 3-52 and described in Table 3-61.
Return to the Summary Table.
Watchdog Control Register
This memory mapped register requires a delay between subsequent writes to the register, otherwise a second write can be lost. The required delay is 69 SYSCLK cycles for a 200 MHz device, 45 SYSCLK cycles for a 120 MHz device, and 39 SYSCLK cycles for a 100 MHz device. This delay can be realized by adding NOP instructions corresponding to the required delay cycles.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | WDPRECLKDIV | ||||||
R-0-0h | R/W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
WDFLG | WDDIS | WDCHK | WDPS | ||||
R/W1S-0h | R/W-0h | R-0/W-0h | R/W-0h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-12 | RESERVED | R-0 | 0h | Reserved |
11-8 | WDPRECLKDIV | R/W | 0h | Watchdog Clock Pre-divider These bits determine the watchdog clock pre-divider, which is the first of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK). The frequency of WDCLK is given by the formulas: PREDIVCLK = INTOSC1 / Pre-divider WDCLK = PREDIVCLK / Prescaler Reset type: IORSn 0h (R/W) = PREDIVCLK = INTOSC1 / 512 1h (R/W) = PREDIVCLK = INTOSC1 / 1024 2h (R/W) = PREDIVCLK = INTOSC1 / 2048 3h (R/W) = PREDIVCLK = INTOSC1 / 4096 4h (R/W) = Reserved 5h (R/W) = Reserved 6h (R/W) = Reserved 7h (R/W) = Reserved 8h (R/W) = PREDIVCLK = INTOSC1 / 2 9h (R/W) = PREDIVCLK = INTOSC1 / 4 Ah (R/W) = PREDIVCLK = INTOSC1 / 8 Bh (R/W) = PREDIVCLK = INTOSC1 / 16 Ch (R/W) = PREDIVCLK = INTOSC1 / 32 Dh (R/W) = PREDIVCLK = INTOSC1 / 64 Eh (R/W) = PREDIVCLK = INTOSC1 / 128 Fh (R/W) = PREDIVCLK = INTOSC1 / 256 |
7 | WDFLG | R/W1S | 0h | Watchdog reset status flag bit. This bit, if set, indicates a watchdog reset (WDRSTn) generated the reset condition. If 0, then it was en external device or power-up reset condition. This bit remains latched until the user writes a 1 to clear the condition. Writes of 0 will be ignored. Reset type: IORSn |
6 | WDDIS | R/W | 0h | Watchdog Disable Setting this bit disables the watchdog module. Clearing this bit enables the watchdog module. This bit can be locked by the WDOVERRIDE bit in the SCSR register. The watchdog is enabled on reset. Reset type: IORSn |
5-3 | WDCHK | R-0/W | 0h | Watchdog Check Bits During any write to this register, these bits must be written with the value 101 (binary). Writing any other value will immediately trigger the watchdog reset or interrupt. Reset type: IORSn |
2-0 | WDPS | R/W | 0h | Watchdog Clock Prescaler These bits determine the watchdog clock prescaler, which is the second of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK). The frequency of WDCLK is given by the formulas: PREDIVCLK = INTOSC1 / Pre-divider WDCLK = PREDIVCLK / Prescaler The watchdog reset or interrupt pulse is 512 INTOSC1 cycles long, so the counter period must be longer. To guarantee this, the product of the prescaler and pre-divider must be greater than or equal to four. The default prescaler value is 1. Reset type: IORSn 0h (R/W) = WDCLK = PREDIVCLK / 1 1h (R/W) = WDCLK = PREDIVCLK / 1 2h (R/W) = WDCLK = PREDIVCLK / 2 3h (R/W) = WDCLK = PREDIVCLK / 4 4h (R/W) = WDCLK = PREDIVCLK / 8 5h (R/W) = WDCLK = PREDIVCLK / 16 6h (R/W) = WDCLK = PREDIVCLK / 32 7h (R/W) = WDCLK = PREDIVCLK / 64 |
WDWCR is shown in Figure 3-53 and described in Table 3-62.
Return to the Summary Table.
Watchdog Windowed Control Register
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | FIRSTKEY | ||||||
R-0-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
MIN | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-9 | RESERVED | R-0 | 0h | Reserved |
8 | FIRSTKEY | R | 0h | This bit indicates if the 1st valid WDKEY (0x55 + 0xAA) got detected after MIN was configured to a non-zero value 0: First Valid Key after non-zero MIN configuration has not happened yet 1: First Valid key after non-zero MIN configuration got detected Notes: [1] If MIN = 0, this bit is never set [2] If MIN is changed back to 0x0 from a non-zero value, this bit is auto-cleared [3] This bit is added for debug purposes only Reset type: IORSn |
7-0 | MIN | R/W | 0h | Watchdog Window Threshold These bits specify the lower limit of the watchdog counter reset window. If the counter is reset via the WDKEY register before the counter value reaches the value in this register, the watchdog immediately triggers a reset or interrupt. Reset type: IORSn |