SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
The instruction memory supports up to eight instructions per event. Each instruction sequence gets triggered on the rising edge of the corresponding event. Starting with CLB Type 2, the option to trigger the execution of instructions using both falling edge and rising edge is available.
The HLC memory supports up to eight instructions per event, starting at the beginning of the fixed address range shown in Table 12-11. An instruction sequence is triggered on the rising edge of the corresponding event. If two or more events occur simultaneously, the associated instruction sequences each are executed sequentially in priority order.
Address | Instructions for |
---|---|
00000 to 00111 | Event 0 |
01000 to 01111 | Event 1 |
10000 to 10111 | Event 2 |
11000 to 11111 | Event 3 |
The HLC instruction format is shown in Table 12-12.
Last Instruction Bit | 5-Bit Opcode | 3-Bit Source | 3-Bit Destination |
---|---|---|---|
This bit when set to 1 stops execution after the current instruction. | MOV 00000 MOV_T1 00001 MOV_T2 00010 PUSH 00011 PULL 00100 ADD 00101 SUB 00110 INTR 00111 | Source can be R0, R1, R2, R3, C0, C1, C2. | Destination can be R0, R1, R2, R3, C0, C1, C2. |
Note that for ADD/SUB instructions, only R0, R1, R2, or R3 can be the destination. |
R0, R1, R2, and R3 are four 32-bit general-purpose registers in the HLC. C0, C1, and C2 are three counter registers present in the CLB tile. <Src> is used to indicate the source and <Dest> is used to indicate the destination. Table 12-13 describes the HLC instructions.
Instruction | Description |
---|---|
ADD <Src>, <Dest> | This instruction performs an unsigned 32-bit addition. <Dest> = <Dest> + <Src>. The <Src> can be R0, R1, R2, R3, C0, C1, or C2. The <Dest> can only be R0, R1, R2, or R3. |
INTR <6-bit constant> | This instruction flags an interrupt through the CPU interface. The 6-bit constant is stored
in the interrupt flag register CLB_INTR_TAG_REG. If multiple INTR
instructions are called consecutively, only the first one has an
effect. When multiple INTR calls are needed, each can be separated
by other HLC instructions to make sure the interrupt calls take
effect. Note: Starting with CLB Type 2, NMI can be generated by the CLB. This
feature is DISABLED by default and must be enabled
(CLB_LOAD_EN.NMI_EN). |
MOV <Src>, <Dest> | This instruction moves <Src> to <Dest>. Both <Src> and <Dest> can be any of R0, R1, R2, R3, C0, C1, or C2. The COUNT_EVENT_CTRL_x bit must be configured to load (that is, 0) for indirect loads and HLC loads of the counter to take effect. |
MOV_T1 <Src>, <Dest> | This instruction moves <Src> to the Match1 register of the <Dest> counter. <Src> can be any of the registers R0, R1, R2, R3, or the counter values associated with C0, C1, or C2. <Dest> is the Match1 register of any of the counters C0, C1, or C2. Examples are:
|
MOV_T2 <Src>, <Dest> | This instruction is similar to MOV_T1. The instruction moves <Src> to the Match2 register of the <Dest> counter. <Src> can be any of the registers R0, R1, R2, R3, or the counter values associated with C0, C1, or C2. <Dest> is the Match2 register of any of the counters C0, C1, or C2. |
PULL <Dest> | This instruction transfers data from the data exchange pull memory buffer in the CPU interface to the <Dest> register. <Dest> can be any of R0, R1, R2, or R3. The PULL instruction is used as seen from the High Level Controller and a PULL operation reads (pulls) data from an internal 4-word FIFO. |
PUSH <Src> | This instruction transfers data from <Src> to the data exchange push memory buffer in the CPU interface. <Src> can be any of R0, R1, R2, R3, C0, C1, or C2. The PUSH instruction is used as seen from the High Level Controller and pushes data into an internal 4 word FIFO. |
SUB <Src>, <Dest> | This instruction performs an unsigned 32-bit subtraction. <Dest> = <Dest> - <Src>. The <Src> can be R0, R1, R2, R3, C0, C1, or C2. The <Dest> can only be R0, R1, R2, or R3. |
MOV, MOV_T1, MOV_T2, ADD, SUB, and INTR instructions take one cycle to execute. PUSH and PULL require two cycles to execute. Note that the PUSH and PULL instructions are pipeline protected, meaning that a register can be used immediately after a PUSH/PULL to that register.
For multiple events triggered simultaneously, if the last instruction in the higher priority event is a PUSH or a PULL, there is an additional cycle delay between the end of the higher priority event and the start of the next event. If the last instruction is not a PUSH or PULL, then there is no cycle delay between the events.