SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
FILE: can_ex6_error_generation.c
This example demonstrates the ways of handling CAN Error conditions It generates the CAN Packets and sends them over GPIO It is looped back externally to be received in CAN module The CAN Interrupt service routine reads the Error status and demonstrates how different Error conditions can be detected
Change ERR_CFG define to the different Error Scenarios and run the example. The corresponding Error Flag will be set in status variable of canaISR() routine. Uses a CPU Timer(Timer 0) for periodic timer interrupt of CANBITRATE uSec On the Timer interrupt it sends the required CAN Frame type with the specified error conditions CAN modules on the device need to be connected to via CAN transceivers. Please refer to the application note titled "Configurable Error Generator for Controller Area Network" at Configurable Error Generator for Controller Area Network for further details on this example
External Connections
Watch Variables Transmit \Configuration