SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
There are two copies of the ePIE vector table. The primary vector table is located at addresses 0xD00 - 0xEFF. The redundant vector table is located at addresses 0x01000D00 - 0x01000EFF. A write to a primary vector address writes to both tables, while a write to a redundant vector address only writes to the redundant table. Both tables are read independently.
During a vector fetch, the ePIE performs a hardware comparison of both vector table outputs. If there is a mismatch between the two vector tables, the CPU branches to the address in the PIEVERRADDR register and the ePIE sends trip signals to the PWMs. If the PIEVERRADDR register value has not been set, the default boot ROM handler at address 0x003FFFBE is used.