SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
To get started using the HIC, first map out the pins needed for the application. See the device data sheet for the set of HIC pins available on the device.
In addition, read the Enabling Peripheral Expansion Applications Using the HIC Application Report before getting started with using the HIC in an application. The application report contains examples of use-cases and is written from an application point of view. Some of the content in this chapter is repeated in the application report. This is done to make sure the application report is a standalone document.