SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
FILE: bgcrc_ex2_cpubgcrc_basic.c
This example demonstrates how to configure and trigger BGCRC from the CPU. It also showcases how to configure the CRC watchdog and lock the registers after configuring the module. The watchdog is used as a diagnostic to check memory test completion within the expected time window. An error signal is generated if the test does not complete in the specified time window.
The module is configured for 1kB of GS0 RAM which is programmed with random data. The golden CRC value for comparison is computed using software method. Interrupt is generated once the computation is done and checks if no error flags are raised. The NMI is enabled and is triggered if an error is detected.
External Connections
Watch Variables