This use case demonstrates a scenario for an application using one boot mode select pin to select between booting to Flash or using CAN boot.
- Program the BOOTPIN_CONFIG location in OTP as follows:
- Set BOOTPIN_CONFIG.BMSP0 to a user specified GPIO, such as 0x0 for GPIO0
- Set BOOTPIN_CONFIG.BMSP1 to 0xFF
- Set BOOTPIN_CONFIG.BMSP2 to 0xFF
- Set BOOTPIN_CONFIG.KEY to 0x5A for boot ROM to treat these register bits as valid and use the custom boot table.
- Program the BOOTDEF location options for the device. This essentially sets up a device-specific boot mode table. Refer to Section 4.7.7 for valid BOOTDEF values to set in the table.
- Set BOOTDEF.BOOTDEF0 to 0x02 for CAN booting. This sets CAN boot to boot table index 0.
- Set BOOTDEF.BOOTDEF1 to 0x03 for booting to Flash (entry address option 0). This sets Flash boot to boot table index 1.
Table 4-8 One Boot Pin Boot Table ResultBoot Mode Table Number | Boot Mode |
---|
0 | CAN Boot (0x02) |
1 | Flash Boot (0x03) |