SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
After the data read unit reads a block of data, the data read unit feeds this data to the CRC-32 compute unit. This unit computes the CRC-32 using the standard polynomial 0x04C11DB7 (x32 + x26 + x23 + x22 + x16 + x12 + x11 + x10 + x8 + x7 + x5 + x4 + x2 + x + 1). The CRC-32 unit retrieves 32-bit of data at a time from the block of data to compute the polynomial. This computation takes 1 cycle. For instance, the CRC-32 calculation for 1KB block of data is 256 cycles, 1 cycle for each of the 256 32-bit chunks. The initial value for the CRC-32 computation can be configured using BGCRC_SEED.
After the CRC-32 calculation is complete for a data block, the final result is loaded into BGCRC_RESULT. Note that BGCRC_RESULT only contains the final calculation for the whole data block; intermediate 32-bit calculations do not update BGCRC_RESULT. The value in BGCRC_RESULT is compared against the value in BGCRC_GOLDEN by hardware and the NMI/Interrupt flags are set accordingly by the CRC notification unit.
Once CRC-32 calculation is commenced, the calculation can be halted by setting BGCRC_CTRL2.TEST_HALT to 1010. Clearing this bit resumes CRC-32 calculation from the halt point.