SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The first write to an idle proxy puts the proxy into write mode for the selected target and channel. Further legal writes are stored in the buffer for the enabled bytes and position within the buffer. A write to a previously written location will overwrite the previous data. When there is a legal write to the last byte of the resource, then the entire data is written by the proxy to the target and channel as a single write burst. The proxy will wait for the write status from the target write before it sends the write status for this final byte host write. This allows the host to use the write status to guarantee the entire write data from the proxy has landed at the target. The proxy is then put back into idle state.