SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
If an error is detected in a proxy thread, the proxy will put that proxy thread into error state, and the current buffer will be lost. A status bit will be set that indicates the proxy thread is in error. All accesses to that proxy thread will be ignored until the status bit is cleared. Once cleared the proxy thread is put back into idle state. Errors are: an access to an offset beyond the length of the message, or a mismatch in the direction of access against what was programmed such as reading an outbound thread or writing an inbound thread.