SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The DDR controller contains a command queue which uses a placement algorithm to determine the order of commands to be placed into the command queue. The placement logic follows many rules to determine where new commands should be inserted into the queue, relative to the contents of the command queue at a time. Placement is determined by considering address collisions, source collisions, data collisions, command types and priorities. The placement logic also attempts to maximize efficiency of the DDR controller through command grouping and bank splitting.