SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
A submission error is returned for a TR that is received that cannot be run. The STATUS_INFO field specifies the type of submission errors.
Value | Submission Error Type |
---|---|
0 | ICNT0 was 0 |
1 | Channel FIFO was full when TR received |
2 | Channel is not owned by the submitter. Either CC submitting to Direct or Direct submitting to a CC channel |
3-15 | Reserved |