SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Figure 6-114 shows the micro-architecture of the polyphase filter data path. The 5-tap filter structure can be programmed to perform a 5-tap Gaussian filter (for Octave generation) or a 4-tap bi-cubic downscaling filter (for scale generation). Or, it can be configured to perform a custom convolution filter without resizing. Filter coefficients for any unused taps should be set to 0. For example, in case of a 4-tap filtering, C2(Fi) filter coefficient should be set to 0. For 3-tap filtering, C-2(Fi) and C2(Fi) filter coefficients should be set to 0.
Kernel Size Configuration
There is no separate configuration required to set the filter kernel size (number of taps) within the polyphase filter. The filter always works as a 5-tap filter but requires unused taps to be masked using the zero coefficients.
Coefficient Precision Selection
The precision of the coefficients is user-configurable using VPAC_MSC_CORE_CFG_j[21-18] COEF_SHIFT which determines the number of fractional bits of the coefficient.
Unsigned/Signed Data Type support
Typically for image resizing, the input and output data are in unsigned (positive) integer numbers in the range of [0..4095]. But, in some non-image convolution filtering (for example, Sobel filter), the input and output data may be in signed integer data format. The MSC supports a user-selectable data type mode bit (VPAC_MSC_CORE_CFG_j[22] SIGNED_DATA) per resizer to specify whether the input/output data is in signed or unsigned data format. The selection determines the input range and output clipping limits as shown below:
VPAC_MSC_CORE_CFG_0[22] SIGNED_DATA = 0 ->[0..4095]
VPAC_MSC_CORE_CFG_0[22] SIGNED_DATA = 1 -> [-2048..2047]
Note that all filters in the same processing thread should have the SIGNED_DATA bit set to a same value.
Rounding Logic
The rounding is done by “adding 0.5 and dropping fractional bits”. This achieves the following:
For data >= 0: “round to nearest, ties away from zero”
For data < 0: “round to nearest, ties toward zero”
This rounding is applied to the 12-bit MSC filter output data. If the result of a filter output is to be stored in SL2 as 8-bit data, an additional rounding in LSE output channel can be optionally enabled to apply rounding during 12bit to 8bit mapping (instead of simple truncation). See DST_BUF_CFG. enable_output_pixel_rounding in LSE_CFG.
Output Saturation Logic
For some non-image unsigned data filtering, the result of the final adder could be negative numbers. To avoid clipping all negative numbers to 0, the MSC filter data processing supports a mode (VPAC_MSC_CORE_CFG_j[22] SAT_MODE = 1) to offset the result by 2048 and then clip the final result to [0..4095] in the output saturation logic to preserve the full data range.
Edge Pixel Replication
Pixel replication in vertical direction (edge line replication) is done in the MSC_LSE.
Pixel replication in horizontal direction (edge pixel replication) is performed in the horizontal filter. For chroma data plane, Cb/Cr pixel replication is done independently with edge Cb/Cr data respectively.