SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The interrupt router (INTRTR) module provides a mechanism to mux M interrupt inputs to N interrupt outputs, where all M inputs are selectable to be driven per N ouput. There is one register per output (MUXCNTL_N) that controls the selection.
There are several INTRTR modules in the device. Their purpose is described in Interrupt Architecture.
The user should take the following into account when programming the MUXCNTL_N register:
The recommended general programming sequence is as follows: