SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The Saturation block first applies a dynamic white balance offset to correct the saturation plane when the image is in log domain and is used for analytics data flow. Once the WB offset is applied, the saturation calculation proceeds as described below. Note that the White balance offset is only applied if the independent pixel values are below a threshold (VISS_FCP_FCC_RGBHSV_WB_LINLOGTHR_1/2). Further, even the minimum of RGB is compared against a threshold (VISS_FCP_FCC_RGBHSV_WB_LINLOGTHR_2[27-16] SATMINTHR bit field) and the higher of the two is used. The saturation calculation always uses the data with the WB correction applied, however the V calculation can choose between WB corrected or uncorrected data using VISS_FCP_FCC_CFG_1[26] MUXRGBHSV_MUX_V.
Table 6-68 shows the condensed form for the Grey Scale and Saturation calculation. In the Flexible CC the saturation calculation is supported using two modes based on the VISS_FCP_FCC_CFG_2[6] HSVSATMODE bit as follows.
Similarly the denominator for the dvision is chosen using the following selection on the VISS_FCP_FCC_CFG_2[5-4] HSVSATDIVMODE bit field.