Instantiated in the MCU domain one Navigator subsystem named MCU_NAVSS can be used for efficient transfer of data support between software, firmware and hardware in all combinations. It consists of the following main modules:
- Unified DMA Controller with the following main modes and features:
- K3 DMA Architecture compliant Tx/Rx port implementation
- K3 DMA Architecture compliant Packet-Oriented DMA Functionality (UDMA-P)
- K3 DMA Architecture compliant Third Party Channel Controller
- K3 DMA Architecture compliant Unified Transfer Controller
- K3 DMA Architecture compliant Unified DMA channels which all share the execution hardware using time division multiplexing
- Ring Accelerator provides hardware acceleration to enable straightforward passing of work between a producer and a consumer and has the following main features:
- Supports 286 independent memory-mapped ring structures
- Supports various modes for each ring based on usage and compatibility
- Provides single-word deep shared incoming Transfer Response FIFO
- Provides bit-wide source VBUSM read/write slave interface for accesses from DMA controller entities
- Proxy module with the following main features:
- Provides proxy buffers to store large data bursts that a host can only access in smaller amounts
- Keeps the large data coherent until the complete data has been accessed
- Allows interleaved access between multiple hosts using multiple proxies
- Supports a pre-configured number of target resources to proxy with pre-configured number of channels, size of each channel, and address offset per each target
- Secure proxy module is a modified version of the proxy module and in addition has the following main features:
- Supports a number of threads, where each has their own independent proxy function
- Supports a programmable fixed queue for each proxy thread
- Supports multiple producers all writing to the same queue
- Supports programmable thresholds for when to generate events
- Supports a max message count for outbound proxy threads limiting the number of messages a thread can produce
- Interrupt Aggregator module provides a centralized machine which handles the termination of system events to that they can be coherently processed by the host(s) in the system. Main features are as follows:
- 64-bit VBUSP slave using 64-bit registers
- Provide a set of TI Interrupt Architecture compliant interrupt status and mask registers which are used to pass specific event status to one or more host blocks
- Provide a set of Global Event Input (GEVI) counters which can count events delivered via an ingress Event Transport Lane (ETL)
- Provides a set of Local Event Input (LEVI) to Global event registers which can be used to convert pulsed discrete interrupt inputs or clock synchronous rising edge events into Global events on an egress ETL
- Provides a set of GEVI 'Multicast' registers which can take a Global event from an ingress ETL and generate two egress Global events on two egress ETL interfaces
- Time Sync module to facilitate host control of time sync operations with the following main features:
- Supports a selection of multiple external clock sources
- Software control of time sync events via interrupt or polling
- Supports 8 hardware timestamp push inputs
- Supports timestamp counter compare output
- Supports timestamp counter bit output
- Supports 6 timestamp generator function outputs
- 32-bit and 64-bit timestamp modes
- Memory Cyclic Redundancy Check module performs CRC to verify the integrity of a memory system with the following main features:
- Four channels to perform background signature verification on any memory subsystem
- Data compression on 8-, 16-, 32-, and 64-bit data size
- Dedicated CRC value register per channel which contains the pre-determined CRC value
- Timed base event trigger from timer to initiate DMA data transfer
- Programmable 20-bit pattern counter per channel to count the number of data patterns for compression
- Three modes of operation: Auto, Semi-CPU, and Full-CPU
- Timeout interrupt generation if CRC is not performed within the time limit
- Per channel DMA request generation to initiate CRC value transfer