SPRUIL1D May 2019 – December 2024 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
The DSI command control for a tearing effect request can be performed using the polling method or automatically. The enable bits for BTA and TE must be enabled for the mechanism to be performed with either the SDI or DIRCMD interface. For automatic operation, the DSI will send a first BTA, and then waits for BTA reception and if no TE has been received during the first BTA(1), it sends another BTA and then waits for TE. There are three possible error conditions that can happen (but only the two first are detected by the DSITX controller and passed to registers):
For the polling method to request a tearing effect (TE polling mode is enabled with te_hw_polling_en = 1) the DSI sends a first BTA, waits for peripheral TE + BTA, if only BTA has been received after the first BTA, it keeps sending BTAs until peripheral responds to the BTA by a TE + BTA instead of BTA only; in this specific mode reg_err_no_te will never be asserted. To stop sending BTA and waiting for TE a force stop(3)) is needed.
Note 1: TE received is checked on the first BTA in case a BTA was the last command issued by the DSI link (BTA or read command sent via direct command interface).
Note 2: Again to support the cases where a BTA was emitted just before the TE request, the TE windows is counted on the first BTA (in case the display understands this BTA as the TE request and thus may emits too late the TE), and is restarted after the second BTA.
Note 3: The time to wait before forcing a stop should be around the duration of a frame. The reason is that if you miss the TE time at the end of the current frame, you've to wait till the end of the next frame before new TE can be sent by display.
The following table describes the TE timeout counter operation, Programming of the IP. The counter value should be calculated based on the tx_byte_clk period.
| te_timeout(11) | te_timeout(10) | timeout value |
|---|---|---|
| 0 | 0 | 256 × te_timeout<9:0> |
| 0 | 1 | 512 × te_timeout<9:0> |
| 1 | 0 | 1024 × te_timeout<9:0> |
| 1 | 1 | 2048 × te_timeout<9:0> |