SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
If clock domain A has a master module that can access a slave module in clock domain B, then clock domain A can have a static dependency with clock domain B. Similarly, a static dependency can also exist between domain A and B if domain B conveys the transactions from a domain A module toward a module in any other domain. For example, CD_DSP can have a static dependency with CD_L3_MAIN1 because this domain has a level 3 (L3) interconnect to carry the transactions from the digital signal processor (DSP) module.
This static dependency consists of forcing clock domain B to stay active as long as there is at least one master module of clock domain A that is not in STANDBY state. If clock domains A and B are initially in GATED state, then clock domain B becomes active as soon as clock domain A becomes active when a wake-up request from the master module is received by the PRCM module.
Similarly, as a result of the static dependency, clock domain B can be gated only if all the master modules of clock domain A that can access the slave modules in clock domain B are in STANDBY state.
The static dependency between a source clock domain and a destination clock domain is configured in the PRCM module by setting the CM_<Source Clock domain>_STATICDEP[x] <Destination Clock domain>_STATDEP bit. As a result, the source clock domain forces the destination clock domain to become active and stay active as long as the source clock domain is active.
The destination domain must be put into forced wake-up (CM_<X>_CLKSTCTRL[1:0] CLKTRCTRL = SW_WKUP) before changing a configurable static dependency.