SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Because the size of the page is 4kiB, any 128-MiB object container is a set of 32,768 pages, organized in an array of 256 columns and 128 rows, as shown in Figure 15-13.
Figure 15-13 Object Container Geometry With 4-kiB PagesThis array of pages is mapped to the system address space, as shown in Figure 15-14.
Figure 15-14 TILER Page Mapping When Using 4-kiB PagesIn any 128-MiB object container, the 4-kiB page Px,y at column x (where 0 =< x < 256) and row y (where 0 =< y < 128), is found at an offset of 4096.(x+256.y) bytes from the base address of the related object container.
Similarly, the page Px,y at column x (where 0 =< x < 256) and row y (where 0 =< y < 128), is translated by the LUT entry Ex+256.y found at the index x+256.y.