SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Another feature of intermediate transfer chaining EDMA_TPCC_OPT_n[23] ITCCHEN is for breaking up large transfers. A large transfer may lock out other transfers of the same priority level for the duration of the transfer. For example, a large transfer on queue 0 from the internal memory to the external memory using the EMIF may starve other EDMA transfers on the same queue. In addition, this large high-priority transfer may prevent the EMIF for a long duration to service other lower priority transfers. When a large transfer is considered to be high priority, it should be split into multiple smaller transfers. Figure 16-51 shows the EDMA setup and illustration of an example single large block transfer.
Figure 16-51 Single Large Block Transfer ExampleThe intermediate transfer chaining enable EDMA_TPCC_OPT_n[23] ITCCHEN provides a method to break up a large transfer into smaller transfers. For example, to move a single large block of memory (16K bytes), the EDMA performs an A-synchronized transfer. The element count is set to a reasonable value, where reasonable derives from the amount of time it would take to move this smaller amount of data. Assume 1 Kbyte is a reasonable small transfer in this example. The EDMA is set up to transfer 16 arrays of 1 Kbyte elements, for a total of 16K byte elements. The EDMA_TPCC_OPT_n[17:12] TCC field in the channel options parameter (OPT) is set to the same value as the channel number and EDMA_TPCC_OPT_n[23] ITCCHEN are set. In this example, EDMA channel 25 is used and EDMA_TPCC_OPT_n[17:12] TCC is also set to 25. The EDMA_TPCC_OPT_n[20] TCINTEN may also be set to trigger interrupt 25 when the last 1 Kbyte array is transferred. The CPU starts the EDMA transfer by writing to the appropriate bit of the event set register EDMA_TPCC_ESR[25] E25. The EDMA transfers the first 1 Kbyte array. Upon completion of the first array, intermediate transfer complete code chaining generates a synchronization event to channel 25, a value specified by the EDMA_TPCC_OPT_n[17:12] TCC field. This intermediate transfer completion chaining event causes EDMA channel 25 to transfer the next 1 Kbyte array. This process continues until the transfer parameters are exhausted, at which point the EDMA has completed the 16K byte transfer. This method breaks up a large transfer into smaller packets, thus providing natural time slices in the transfer such that other events may be processed. Figure 16-52 shows the EDMA setup and illustration of the broken up smaller packet transfers.
Figure 16-52 Smaller Packet Data Transfers Example