SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The DMM manages its internal memory space as an ordered set of up to four sections. Figure 15-5 shows the DMM sections and memory mapping.
Figure 15-5 DMM Sections and Memory MappingIn the DMM, a section is:
Each of the four sections is configured through a DMM_LISA_MAP_i register, where i = 0 to 3.
The DMM and EMIF registers (see EMIF Controller) are declared in two extra static DMM sections of the highest priority so that they cannot be masked by any standard programmable DMM section.
The DMM atomic size is 1KiB.