SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Although the previous configuration allows the EDMA to service a peripheral continuously, it presents a number of restrictions to the CPU. Because the input and output buffers are continuously being filled/emptied, the CPU must match the pace of the EDMA very closely to process the data. The EDMA receive data must always be placed in memory before the CPU accesses it, and the CPU must provide the output data before the EDMA transfers it. Though not impossible, this is an unnecessary challenge. It is particularly difficult in a 2-level cache scheme.
Ping-pong buffering is a simple technique that allows the CPU activity to be distanced from the EDMA activity. This means that there are multiple (usually two) sets of data buffers for all incoming and outgoing data streams. While the EDMA transfers the data into and out of the ping buffers, the CPU manipulates the data in the pong buffers. When both CPU and EDMA activity completes, they switch. The EDMA then writes over the old input data and transfers the new output data. Figure 16-46 shows the ping-pong scheme for this example.
To change the continuous operation example, such that a ping-pong buffering scheme is used, the EDMA channels need only a moderate change. Instead of one parameter set, there are two; one for transferring data to/from the ping buffers and one for transferring data to/from the pong buffers. As soon as one transfer completes, the channel loads the PaRAM set for the other and the data transfers continue. Figure 16-47 shows the EDMA channel configuration required.
Each channel has two parameter sets, ping and pong. The EDMA channel is initially loaded with the ping parameters (Figure 16-47). The link address for the ping set is set to the PaRAM offset of the pong parameter set (Figure 16-48). The link address for the pong set is set to the PaRAM offset of the ping parameter set (Figure 16-49). The channel options, count values, and index values are all identical between the ping and pong parameters for each channel. The only differences are the link address provided and the address of the data buffer.
Figure 16-46 Ping-Pong Buffering for McASP Data Example