SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The trimmer can be programmed to re-define a new source image within the input video frame sent from an upstream module before it is sent to the scaling sub-modules. This feature enables small area zoom out, source pan/scan, or removal of unwanted area in the video (such as black box / curtains / noisy line-21 video) without modifying the VPDMA parameters.
Horizontal and vertical offset is set through VIP_CFG_SC25[26:16] CFG_OFF_W and VIP_CFG_SC25[10:0] CFG_OFF_H registers.
Width and height are set through VIP_CFG_SC24[26:16] CFG_ORG_W and VIP_CFG_SC24[10:0] CFG_ORG_H registers.
Figure 9-81 Input Image TrimmingWidth and height of the source image are global parameters and are set with VIP_CFG_SC5[22:12] CFG_SRC_W and VIP_CFG_SC5[10:0] CFG_SRC_H registers.
It is required that the input image frame (CFG_SRC_W x CFG_SRC_H) to be at least 32 × 32 (after trimming, if the trimming is enabled) to properly fill the input filter stage pipelines.