SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The SCP interface of the SATA PLL controller (the DPLLCTRL_SATA instance) is used to set the configuration of the digital phase-locked loop (DPLL) modules, primarily the various counter values. Figure 26-4 is an overview of the DPLL clock generator embedded into the SATA host controller subsystem.
Figure 26-4 SATA DPLL Clock Generator OverviewThe DPLLCTRL_SATA module is user accessible on the L4_CFG interconnect. However, to make access possible, the user must configure the OCP2SCP3 instance prior to accessing the DPLLCTRL_SATA registers.
The DPLL_SATA features are:
The DPLLCTRL_SATA components features are: