SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
When running with the default PMCU configuration, timers and serial interfaces can select either the bus clock (MCLK/ULPCLK) or the LFCLK as their clock source. LFCLK is always 32kHz in RUN, SLEEP, STOP, and STANDBY, but MCLK/ULPCLK changes to 4MHz in STOP and to 32kHz in STANDBY, meaning that peripherals running from the bus clock see the source clock frequency change when transitioning power modes.
MFCLK, by contrast, works like LFCLK in that it provides a constant frequency clock source for peripherals across RUN, SLEEP, and STOP modes. MFCLK provides a constant 4MHz as an alternative to LFCLK which runs at 32kHz. The 4MHz time base for MFCLK is always derived from SYSOSC. Peripherals, specifically PD0 peripherals that can be used in STOP mode, can select MFCLK as their clock source instead of ULPCLK. MFCLK is maintained at 4MHz in RUN, SLEEP and STOP for peripherals like UART, I2C, and low-power timers that need a consistent clock but require a clock source greater than 32kHz.
For information on using MFCLK, see the MFCLK section.