SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
There are two settings for the CCP output channel behavior in a fault condition, TIMA.CCACT_01[0/1].FEXACT (fault exit behavior) and TIMA.CCACT_01[0/1].FENACT (fault entry behavior). The output behavior of fault condition is described in Table 28-22.
| Bit Fields | Output Behavior | |
|---|---|---|
| FEXACT | FENACT | |
| 0 | The CCP output value is unaffected by the fault event | |
| 1 | CCP output value is set high | |
| 2 | CCP output value is set low | |
| 3 | CCP output value toggles | |
4 |
CCP output is tristated (Hi-Z) | |
If using the TIMA_FALx pin with the CCP capture channel inputs (such as adding deadband to complimentary PWMs) for low latency actions, an external connection should be in hardware between the TIMA_FALx pin and TIMAx_Cy pin (x = timer instance, y = CC channel).