SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Majority voting provides noise immunity by sampling each bit 3 times in the center of the bit period.
Majority voting is only for data bits. Select majority voting or single sample using the MAJVOTE control bit in the CTL0 register. Disable majority voting if IrDA or Manchester Encoding modes are used.
Example 1: When the UARTx.CTL0.HSE is set to 0 with 16 oversampling; the 7th, 8th and 9th bit are sampled.
Example 2: When the UARTx.CTL0.HSE is set to 1 with 8 oversampling; then the 3rd ,4th and 5th bits are sampled and majority value is considered as final value to be sampled. Oversampling with majority voting is only applicable for 16 and 8 oversampling.
In both examples, the majority value is considered as the final value to be sampled.
When the 3 samples used for majority vote are not equal; the RIS.NE (noise error bit) is set. The received data is transferred despite the noise error. The NE bit appends to the received data before storing NE in the RXDATA register at bit position 12.