SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The following table shows the memory organization for LCDMX=4 to LCDMX=7. Each row of memory corresponds to 1 pin. Each bit in a row corresponds to one of the common slots (COM0 to COM7). For example, if a segment is associated with pin L3 and common COM2, then the bit at row-3 and column-4 needs to be used. If this bit is set, the waveform generated on L3 along with waveform generated on COM3 (one of the other pins) would make the segment glow. In case a particular pin is a common pin (COM0 to COM3) the corresponding bit in the row should be used. For example, if L5 is configured as common pin COM2, then bit at row-5 and column-2 should be set.
| Memory Row | COM7
(MSB-7) |
COM6 | COM5 | COM4 | COM3 | COM2 | COM1 | COM0
(LSB-0) |
|---|---|---|---|---|---|---|---|---|
| 0 | L0 | L0 | L0 | L0 | L0 | L0 | L0 | L0 |
| 1 | L1 | L1 | L1 | L1 | L1 | L1 | L1 | L1 |
| 2 | L2 | L2 | L2 | L2 | L2 | L2 | L2 | L2 |
| 3 | L3 | L3 | L3 | L3 | L3 | L3 | L3 | L3 |
| 4 | L4 | L4 | L4 | L4 | L4 | L4 | L4 | L4 |
| 5 | L5 | L5 | L5 | L5 | L5 | L5 | L5 | L5 |
| 6 | L6 | L6 | L6 | L6 | L6 | L6 | L6 | L6 |
| 7 | L7 | L7 | L7 | L7 | L7 | L7 | L7 | L7 |
| 8 | L8 | L8 | L8 | L8 | L8 | L8 | L8 | L8 |
| 9 | L9 | L9 | L9 | L9 | L9 | L9 | L9 | L9 |
| 10 | L10 | L10 | L10 | L10 | L10 | L10 | L10 | L10 |
| 11 | L11 | L11 | L11 | L11 | L11 | L11 | L11 | L11 |
| 12 | L12 | L12 | L12 | L12 | L12 | L12 | L12 | L12 |
| 13 | L13 | L13 | L13 | L13 | L13 | L13 | L13 | L13 |
| 14 | L14 | L14 | L14 | L14 | L14 | L14 | L14 | L14 |
| 15 | L15 | L15 | L15 | L15 | L15 | L15 | L15 | L15 |
| 16 | L16 | L16 | L16 | L16 | L16 | L16 | L16 | L16 |
| 17 | L17 | L17 | L17 | L17 | L17 | L17 | L17 | L17 |
| 18 | L18 | L18 | L18 | L18 | L18 | L18 | L18 | L18 |
| 19 | L19 | L19 | L19 | L19 | L19 | L19 | L19 | L19 |
| 20 | L20 | L20 | L20 | L20 | L20 | L20 | L20 | L20 |
| 21 | L21 | L21 | L21 | L21 | L21 | L21 | L21 | L21 |
| 22 | L22 | L22 | L22 | L22 | L22 | L22 | L22 | L22 |
| 23 | L23 | L23 | L23 | L23 | L23 | L23 | L23 | L23 |
| 24 | L24 | L24 | L24 | L24 | L24 | L24 | L24 | L24 |
| 25 | L25 | L25 | L25 | L25 | L25 | L25 | L25 | L25 |
| 26 | L26 | L26 | L26 | L26 | L26 | L26 | L26 | L26 |
| 27 | L27 | L27 | L27 | L27 | L27 | L27 | L27 | L27 |
| 28 | L28 | L28 | L28 | L28 | L28 | L28 | L28 | L28 |
| 29 | L29 | L29 | L29 | L29 | L29 | L29 | L29 | L29 |
| 30 | L30 | L30 | L30 | L30 | L30 | L30 | L30 | L30 |
| 31 | L31 | L31 | L31 | L31 | L31 | L31 | L31 | L31 |
| 32 | L32 | L32 | L32 | L32 | L32 | L32 | L32 | L32 |
| 33 | L33 | L33 | L33 | L33 | L33 | L33 | L33 | L33 |
| 34 | L34 | L34 | L34 | L34 | L34 | L34 | L34 | L34 |
| 35 | L35 | L35 | L35 | L35 | L35 | L35 | L35 | L35 |
| 36 | L36 | L36 | L36 | L36 | L36 | L36 | L36 | L36 |
| 37 | L37 | L37 | L37 | L37 | L37 | L37 | L37 | L37 |
| 38 | L38 | L38 | L38 | L38 | L38 | L38 | L38 | L38 |
| 39 | L39 | L39 | L39 | L39 | L39 | L39 | L39 | L39 |
| 40 | L40 | L40 | L40 | L40 | L40 | L40 | L40 | L40 |
| 41 | L41 | L41 | L41 | L41 | L41 | L41 | L41 | L41 |
| 42 | L42 | L42 | L42 | L42 | L42 | L42 | L42 | L42 |
| 43 | L43 | L43 | L43 | L43 | L43 | L43 | L43 | L43 |
| 44 | L44 | L44 | L44 | L44 | L44 | L44 | L44 | L44 |
| 45 | L45 | L45 | L45 | L45 | L45 | L45 | L45 | L45 |
| 46 | L46 | L46 | L46 | L46 | L46 | L46 | L46 | L46 |
| 47 | L47 | L47 | L47 | L47 | L47 | L47 | L47 | L47 |
| 48 | L48 | L48 | L48 | L48 | L48 | L48 | L48 | L48 |
| 49 | L49 | L49 | L49 | L49 | L49 | L49 | L49 | L49 |
| 50 | L50 | L50 | L50 | L50 | L50 | L50 | L50 | L50 |
| 51 | L51 | L51 | L51 | L51 | L51 | L51 | L51 | L51 |
| 52 | L52 | L52 | L52 | L52 | L52 | L52 | L52 | L52 |
| 53 | L53 | L53 | L53 | L53 | L53 | L53 | L53 | L53 |
| 54 | L54 | L54 | L54 | L54 | L54 | L54 | L54 | L54 |
| 55 | L55 | L55 | L55 | L55 | L55 | L55 | L55 | L55 |
| 56 | L56 | L56 | L56 | L56 | L56 | L56 | L56 | L56 |
| 57 | L57 | L57 | L57 | L57 | L57 | L57 | L57 | L57 |
| 58 | L58 | L58 | L58 | L58 | L58 | L58 | L58 | L58 |
| 59 | L59 | L59 | L59 | L59 | L59 | L59 | L59 | L59 |
| 60 | L60 | L60 | L60 | L60 | L60 | L60 | L60 | L60 |
| 61 | L61 | L61 | L61 | L61 | L61 | L61 | L61 | L61 |
| 62 | L62 | L62 | L62 | L62 | L62 | L62 | L62 | L62 |
| 63 | L63 | L63 | L63 | L63 | L63 | L63 | L63 | L63 |