SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
There are three main power domains on MSPM0Lxx devices:
The PD1 domain is disabled in certain operating modes to minimize power consumption. The PD0 domain supports ultra-low-power performance and is always enabled in operating modes in which the core regulator is operating.
There are four main data buses on MSPM0Lxx devices:
The CPU and the DMA controller are the only two bus controllers in the device. Arbitration between the CPU and the DMA for shared peripherals happens between the CPU-only PD1 peripheral bus and the CPU/DMA PD1 peripheral bus. The DMA does not have access to peripherals on the CPU-only PD1 peripheral bus or the CPU bus matrix (the green components in the bus diagram). As such, the CPU can access peripherals on the CPU-only PD1 peripheral bus at the same time that the DMA is processing a transaction on the PD1 or PD0 bus.
Likewise, the CPU can access SRAM or flash memory through the AHB bus matrix at the same time that the DMA is processing a transaction, so long as the DMA is not accessing the same memory that the CPU is attempting to access. Arbitration between the CPU and the DMA for memory systems (SRAM or flash memory) happens at the memory interface itself. All arbitration between the CPU and DMA is done on a round-robin basis.
The GPIO and ADC peripherals (the orange components in the bus diagram) have special capabilities to enable both fast register access from the CPU and operation in low power operating modes.