SLAU847F October 2022 – March 2026 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The BCR supports executing a complete CRC32 integrity check of the application code and data contained in the MAIN flash regions during the boot process before starting the user application. This is useful to ensure the integrity of some or all of the application code and data before executing it.
To enable the CRC32 integrity check at boot, the following information must be programmed into the BCR configuration in NONMAIN flash memory:
In the event that an application CRC check fails at boot, the application in MAIN flash is not started. If the boot strap loader is enabled, it is entered. If the BSL is not enabled, then the boot fails.