SLUAAW1A May 2024 – July 2024 2N7001T , 2N7001T-Q1 , CD4009UB , CD4009UB-MIL , CD40109B , CD40109B-MIL , CD40109B-Q1 , CD4010B , CD4010B-MIL , CD4010B-Q1 , CD4504B , CD4504B-EP , CD4504B-MIL , FPC202 , FPC401 , FPC402 , ISO1540 , ISO1540-Q1 , ISO1541 , ISO1541-Q1 , ISO1640 , ISO1640-Q1 , ISO1641 , ISO1642 , ISO1643 , ISO1644 , LM8330 , LM8333 , LSF0101 , LSF0102 , LSF0102-Q1 , LSF0108 , LSF0108-Q1 , LSF0204 , LSF0204-Q1 , LSF0204D , P82B715 , P82B96 , PCA9306 , PCA9306-Q1 , PCA9515A , PCA9515B , PCA9518 , PCA9534 , PCA9534A , PCA9535 , PCA9536 , PCA9538 , PCA9539 , PCA9554 , PCA9554A , PCA9555 , PCA9557 , PCF8574 , PCF8574A , PCF8575 , SN10KHT5541 , SN10KHT5543 , SN10KHT5574 , SN54SC4T125-SEP , SN54SC6T06-SEP , SN54SC6T07-SEP , SN54SC6T14-SEP , SN54SC6T17-SEP , SN54SLC8T245-SEP , SN74ACT1284 , SN74ALVC164245 , SN74ALVC164245-EP , SN74AUP1T04 , SN74AUP1T14 , SN74AUP1T17 , SN74AUP1T34 , SN74AUP1T34-Q1 , SN74AUP1T50 , SN74AVC16T245 , SN74AVC16T245-Q1 , SN74AVC1T45 , SN74AVC20T245 , SN74AVC24T245 , SN74AVC2T244 , SN74AVC2T245 , SN74AVC2T45 , SN74AVC2T45-Q1 , SN74AVC32T245 , SN74AVC4T234 , SN74AVC4T245 , SN74AVC4T245-Q1 , SN74AVC4T774 , SN74AVC6T622 , SN74AVC8T245 , SN74AVC8T245-Q1 , SN74AVCA164245 , SN74AVCA406 , SN74AVCAH164245 , SN74AVCB164245 , SN74AVCB164245-EP , SN74AVCB164245-Q1 , SN74AVCBH164245 , SN74AVCH16T245 , SN74AVCH1T45 , SN74AVCH20T245 , SN74AVCH24T245 , SN74AVCH2T45 , SN74AVCH4T245 , SN74AVCH4T245-EP , SN74AVCH4T245-Q1 , SN74AVCH8T245 , SN74AXC1T45 , SN74AXC1T45-Q1 , SN74AXC2T245 , SN74AXC2T245-Q1 , SN74AXC2T45 , SN74AXC2T45-Q1 , SN74AXC4T245 , SN74AXC4T245-Q1 , SN74AXC4T774 , SN74AXC4T774-Q1 , SN74AXC8T245 , SN74AXC8T245-Q1 , SN74AXCH1T45 , SN74AXCH2T45 , SN74AXCH4T245 , SN74AXCH8T245 , SN74FB1650 , SN74FB1653 , SN74GTL16612 , SN74GTL16616 , SN74GTL16622A , SN74GTL2003 , SN74GTL2007 , SN74GTL2010 , SN74GTL2014 , SN74GTL2107 , SN74GTL3004 , SN74GTLP1394 , SN74GTLP1395 , SN74GTLP2033 , SN74GTLP21395 , SN74GTLP22033 , SN74GTLP817 , SN74GTLPH1645 , SN74GTLPH1655 , SN74GTLPH16912 , SN74GTLPH16945 , SN74GTLPH306 , SN74LV161284 , SN74LV1T04 , SN74LV1T04-Q1 , SN74LV1T125 , SN74LV1T125-Q1 , SN74LV1T126 , SN74LV1T126-Q1 , SN74LV1T34 , SN74LV1T34-Q1 , SN74LV4T125 , SN74LV4T125-EP , SN74LV4T125-Q1 , SN74LV6T06 , SN74LV6T06-EP , SN74LV6T06-Q1 , SN74LV6T07 , SN74LV6T07-EP , SN74LV6T07-Q1 , SN74LV6T14 , SN74LV6T14-EP , SN74LV6T14-Q1 , SN74LV6T17 , SN74LV6T17-EP , SN74LV6T17-Q1 , SN74LVC161284 , SN74LVC16T245 , SN74LVC16T245-EP , SN74LVC1T45 , SN74LVC1T45-EP , SN74LVC1T45-Q1 , SN74LVC2T45 , SN74LVC2T45-EP , SN74LVC2T45-Q1 , SN74LVC4245A , SN74LVC4245A-EP , SN74LVC8T245 , SN74LVC8T245-EP , SN74LVC8T245-Q1 , SN74LVCC3245A , SN74LVCC3245A-EP , SN74LVCC4245A , SN74LVCC4245A-EP , SN74LVCE161284 , SN74LVCH16T245 , SN74LVCH16T245-EP , SN74LVCH8T245 , SN74LVCZ161284A , SN74LXC1T14 , SN74LXC1T14-Q1 , SN74LXC1T45 , SN74LXC1T45-Q1 , SN74LXC2T45 , SN74LXC2T45-Q1 , SN74LXC8T245 , SN74LXC8T245-Q1 , SN74LXCH1T45 , SN74LXCH8T245 , TCA39306 , TCA39306-Q1 , TCA39416 , TCA4307 , TCA5013 , TCA5405 , TCA6408A , TCA6408A-Q1 , TCA6416A , TCA6418E , TCA6424A , TCA6507 , TCA8418 , TCA8418E , TCA9406 , TCA9416 , TCA9509 , TCA9511A , TCA9517 , TCA9517-Q1 , TCA9517A , TCA9534 , TCA9534A , TCA9535 , TCA9536 , TCA9537 , TCA9538 , TCA9539 , TCA9539-Q1 , TCA9554 , TCA9554A , TCA9555 , TCA9617A , TCA9617B , TCA9800 , TCA9801 , TCA9802 , TCA9803 , TCAL6408 , TCAL6416 , TCAL9538 , TCAL9539 , TCAL9539-Q1 , TWL1200 , TWL1200-Q1 , TXB0101 , TXB0102 , TXB0104 , TXB0104-Q1 , TXB0106 , TXB0106-Q1 , TXB0108 , TXB0302 , TXB0304 , TXH0137D-Q1 , TXS0101 , TXS0102 , TXS0102-Q1 , TXS0104E , TXS0104E-Q1 , TXS0108E , TXS0108E-Q1 , TXS0202 , TXS0206 , TXS0206-29 , TXS0206A , TXS02324 , TXS02326A , TXS02612 , TXS4555 , TXS4558 , TXU0101 , TXU0101-Q1 , TXU0102 , TXU0102-Q1 , TXU0104 , TXU0104-Q1 , TXU0202 , TXU0202-Q1 , TXU0204 , TXU0204-Q1 , TXU0304 , TXU0304-Q1 , TXV0106 , TXV0106-Q1 , TXV0108 , TXV0108-Q1
Two important parameters that characterize the performance of level-shifters are Transient drive strength and DC / Static drive strength. Understanding the differences between these two parameters are essential for selecting the correct level-shifter for system designers.
All trademarks are the property of their respective owners.
Transient drive strength refers to the ability of the CMOS output buffer to deliver high current during short-duration transient events, such as switching transitions. This indicates the ability of the output to supply or sink current by quickly charging or discharging the output capacitance, while switching from LOW to HIGH or HIGH to LOW.
Transient drive strength is critical for ensuring fast rise and fall times of output signals charging and discharging larger capacitive loads, which directly impact the system's speed and signal integrity. A faster rise and fall time indicates a higher transient drive strength. In high-speed applications, such as clock distribution and data transmission, a strong transient drive capability is essential to minimize signal propagation delays for higher loads and reduce the risk of signal distortion.
Design considerations for enhancing transient drive strength includes optimizing the output stage's size – width and length of the transistors used in the pull-up and pull-down buffers and minimizing parasitic capacitance in the output network to increase transient response.
However, careful system considerations are recommended as some systems might not be able to handle strong transient drive due to sensitivities to transmission line effects. Some symptoms can include overshoots / undershoots / reflections (commonly known as ringing). Simply using series dampening resistors on the outputs help adjust accordingly, per system requirements. Appropriate dampening resistor sizing should be considered to accommodate for the reduced rise/fall times, the voltage drop across the resistor limiting the signal swing, additional propagation delay and additional power dissipation introduced.
Rise or Fall times are good indicators of a device’s transient drive strength.
DC / Static drive strength refers to the ability to maintain a stable output voltage level under static steady-state conditions. The DC / Status drive determines the maximum load current that the output buffer can reliably drive without significant voltage droop (not < specified VOH levels) or distortion and is generally measured using IOH and IOL of the buffer.
This is the current needed by the output to source or sink while maintaining the VOH / VOL voltage levels at the specified high-level (logic 1) or low-level (logic 0). Transient drive is significant for how fast the output gets to a logic 1 (rise time) or logic 0 (fall time) while static drive maintains or keeps the output steady for a specified high-level (logic 1) or low-level (logic 0) voltage respectively.
This static current strength is crucial for making sure the stability and reliability of digital systems, especially in applications where the output buffer drives resistive loads, LED loads, and so on.
To enhance static drive strength, designers typically focus on optimizing the biasing conditions of the output transistors and minimizing output impedance across various supply voltages and process parameters.
IOH and IOL are good indicators of a device’s DC drive strength.
While transient current drive strength emphasizes the ability to handle rapid slew rate changes in output voltage, static current drive strength focuses on maintaining voltage levels under steady-state conditions. Both parameters are interrelated but address different aspects of output buffer performance.
It is essential for application or system engineers to balance transient and static current drive strength requirements based on the specific application's speed, load conditions, and power constraints. In some cases, optimizing for one parameter may lead to compromises in the other.
For applications like driving an LED, motor, or driving a I2C device where there is a demand for high static current, system designers can consider static current drive strength. Whereas, rise or fall times act as a measure of transient drive strength when driving capacitive. Therefore, careful consideration and trade-off analysis are necessary during the design phase to meet the desired performance specifications of rise or fall times and static current drive requirements.
To make sure a high static current strength, larger MOSFETs are typically deployed with wider routing and connections to avoid reliability concerns like electro-migration. These large size FETs poses two challenges to designers:
To control ringing, current limiter circuits are added in CMOS buffers to limit the transient current and thus reduce ringing. Hence, the buffer with high static current strength can have a low transient strength.
Figure 4-1 and Figure 4-2 compares SN74AVCxT245 (faster transient drive - rise or fall times, lower static drive - specified for up to 12mA) and SN74LXCxT245 (slower transient drive - rise or fall times, higher static drive - specified for up to 32mA).
Figure 4-1, compares AVC and LXC transient drive strengths. AVC switches faster than LXC, indicating a higher transient drive strength.
Figure 4-4, compares AVC and LXC transient currents required for their switching transitions. Although specified for a lower static current, the faster AVC device requires higher transient currents to switch between the fast HIGH or LOW transitions.
Static current drive strength focuses on providing a strong and steady signal during normal operating conditions. Transient current drive strength emphasizes the ability to quickly and effectively drive the load capacitance during signal transitions. Both static and transient current drive strengths are essential for reliable and high-performance digital system design. However, they both address different aspects of signal integrity and performance.