SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Enables individual I2S interrupt sources.
Parameters:
ulBasethe base address of the I2S module
ulIntFlagsthe bit mask of the interrupt sources to be enabledThis function enables the indicated I2S interrupt sources. Only enabled sources can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The
ulIntFlags
parameter is the logical OR for any of the following:
-I2S_INT_XUNDRN -I2S_INT_XSYNCERR -I2S_INT_XLAST -I2S_INT_XDATA
-I2S_INT_XSTAFRM -I2S_INT_XDMA -I2S_INT_ROVRN -I2S_INT_RSYNCERR
-I2S_INT_RLAST -I2S_INT_RDATA -I2S_INT_RSTAFRM -I2S_INT_RDMAReturns:
None