SWRU543B January 2019 – June 2025
According to the state of the transmitter register and the receiver register, the channel can issue interrupt events if enabled. A status bit in the SPI_IRQSTATUS register of each interrupt event indicates service is required. Each interrupt event contains an interrupt enable bit in the SPI_IRQENABLE register; this bit enables the status to generate hardware interrupt requests. When an interrupt occurs and a mask is then applied on it (IRQENABLE), the interrupt line is not asserted again, even if the interrupt source has not been serviced.
SPI supports interrupt-driven operation and polling.